HRB1684301-15

Accessing the meter webpages

NOTE: Refer to Restoration of temporarily disabled configuration settings in webpages to know availability of these features on your meter model.

Access the meter’s webpages to view data and perform basic configuration and data export tasks using a web browser.

The webpages are accessed through the meter’s Ethernet port so it must be configured properly.

  1. Open web browser and enter the meter’s IP address in the address box.
  2. Enter your Username and Password.

    The Username and Password for the default user accounts are user1 / pass1 and user2 / pass2.

  3. Use the menus and tabs to select and display the meter's various webpages.
  4. Click the up / down arrows to show and hide sections of the webpages and menus.
  5. Click Logout to exit the meter webpages.
QR code for this page

Was this helpful?