Accessing the meter webpages
-
The webpages are accessed through the meter’s Ethernet port so it must be configured properly.
-
It is mandatory to change the default password when you access the webpages for the first time. You cannot browse through the webpages without the default password change.
-
The password must contain between 8 and 16 characters with at least 1 number, 1 capital letter and 1 special character.
- Open a web browser and enter the meter’s IP address in the address box.
-
Enter the Username (default: Administrator) and Password (default:
MAC address which is unique for each meter).
NOTE: Enter the MAC address of the meter without colon in capital letters (For example: if the MAC address of the meter is 00:80:f4:02:14:38, then password is 0080F4021438).
WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITYRecommended to change the default password.Failure to follow these instructions can result in unauthorized personnel accessing the web pages. - Click Login.
-
Use the menus and tabs to select and display the meter's
various webpages.
NOTE: If the user session is inactive for a period of 10 minutes or more, the session gets timed-out and you need to re-login to access the webpages.
- Click Logout to exit the meter webpages.