HRB1684301-13

Analog inputs

The meter is equipped with two analog inputs (A1 & A2)*.

NOTE: *Available in specific meter models. Refer to Features differentiation matrix for PM5500 / PM5600 / PM5700 series for the availability.

The analog inputs interpret an incoming analog current signal from transducers. For analog input operation, the meter processes an analog input signal and provides the resulting scaled value.

The meter measures the current using standard 4 - 20 mA analog transducers.

QR code for this page

Was this helpful?