HRB1684301-12

Configuring DNP3 setting using the webpages

NOTE: Refer to Restoration of temporarily disabled configuration settings in webpages to know availability of these features on your meter model.

You can use the meter’s webpages to configure DNP3 settings.

  1. Login to the meter webpages.
  2. Based on your meter firmware version, click Settings > DNP3 Settings OR click Settings > Communication > DNP3 Settings.
  3. Click Yes to enable DNP3 or click No to disable DNP3 as required.
  4. Click Save changes or Apply Changes to send and save the new settings to the meter.
QR code for this page

Was this helpful?