HRB1684301-15

Configuring the LED for alarms using ION Setup

You can use ION Setup to configure your meter’s LED for alarming.
NOTE: The alarm / energy pulsing LED on the PM5561 / PM5661 / PM5761 is permanently set for energy pulsing and cannot be used for alarms.
  1. Open ION Setup and connect to your meter. See the ION Setup Help for instructions.
  2. Navigate to I/O configuration > Energy Pulsing .
  3. Select Front Panel LED and click Edit.
  4. Set the control mode to Alarm.
  5. Click Send to save your changes.
QR code for this page

Was this helpful?