HRB1684301-12

Configuring the LED for alarms using the display

You can use the meter display to configure the alarm / energy pulsing LED for alarming.
NOTE: The alarm / energy pulsing LED on the PM5561 / PM5661 / PM5761 is permanently set for energy pulsing and cannot be used for alarms.
  1. Navigate to the LED setup menu screen.
  2. Set the mode to Alarm, then press OK.
  3. Press the up arrow to exit. Press Yes to save your changes.
QR code for this page

Was this helpful?