HRB1684301-13

Configuring waveform capture using the display

You can use the display to configure the waveform capture.
  1. Navigate to Maint > Setup.
  2. Enter the setup passcode (default is “0”), then press OK.
  3. Navigate to WFC.
  4. Move the cursor to point to the parameter you want to modify, then press Edit.
  5. Modify the parameters as required, then press OK.
  6. Press the up arrow to exit. Press Yes to save your changes.

    Waveform capture setup parameters available using the display

    Parameter

    Values

    Description

    Enable

    Yes, No

    Enables or disables the waveform capture on your meter

    Samples Per Cycle

    128

    64

    32

    16

    Select the samples per cycle based on the requirement

    Pre Cycles

    The pre cycles can be configured based on the samples per cycle

    • Maximum 1 – 8 pre cycles for 128 samples per cycle

    • Maximum 1 – 16 pre cycles for 64 samples per cycle

    • Maximum 1 – 32 pre cycles for 32 samples per cycle

    • Maximum 1 – 64 pre cycles for 16 samples per cycle

    Select the pre cycles based on the requirement

    The Post-cycles will be automatically configured based on the Pre-cycles

    NOTE: It is recommended for the end user to configure equal number of pre and post cycles to visualize sag/swell events in waveform.

    • Pre-cycles: Number of cycles that will be captured in waveforms prior to waveform trigger

    • Post-cycles : Number of cycles that will be captured in waveforms post waveform trigger

QR code for this page

Was this helpful?