HRB1684301-12

Default settings

NOTE: Refer to Restoration of temporarily disabled configuration settings in webpages to know availability of these features on your meter model.

Area

Setting

Default

Communication protocols

Modbus TCP/IP

Enabled

EtherNet/IP

Enabled

BACnet/IP

Enabled

FTP / FTPS*

Disabled

SNMP

Enabled

SNTP

Disabled

SMTP

Disabled

DNP3

Disabled

HTTP / HTTPS*

Enabled

Time and time keeping

Time synchronization

Disabled

Web browser

Webpages

Enabled

Configuration

Using the Display

Enabled

Using webpages

Enabled

Using Modbus programming

Enabled

* Available only in latest firmware versions:

  • PM5560 / PM5562 / PM5563 / PM5580 meter models: 4.0.0 and above

  • PM5570 / PM5660 / PM5760 meter models: 6.0.0 and above

  • PM5650 meter model: 4.10.0 and above

  • PM5561 meter model: 12.0.0 and above

  • PM5661 / PM5761 meter models: 14.0.0 and above

QR code for this page

Was this helpful?