HRB1684301-12

Diagnostics information

The meter provides you with diagnostics information to help with troubleshooting.

Navigate to Maint > Diag > Info to view the meter model, serial number, date of manufacture, firmware version (including OS - Operating System and RS - Reset System), language version, and OS CRC (Cyclic Redundancy Check). The OS CRC value is a number (Hexadecimal format) that identifies the uniqueness between different OS firmware versions.

Navigate to Maint > Diag > Meter to view details of the meter status.

Navigate to Maint > Diag > Cl Pwr to view the control power information.

  • Non-MID meter models: The Cl Pwr screen displays how many times the meter lost control power, and the date and time of its last occurrence.

  • MID meter models: The Cl Pwr screen displays the Number of Losses, the Last Power Up and the Last Power Down events with the timestamp.

Navigate to Maint > Diag > Phasor to view the graphical representation of the power system the meter is monitoring.

Navigate to Maint > Diag > Phasor > Polar to view the numeric magnitude and angles of all voltage and current phases.

You can access the meter’s maintenance log using the webpages.

QR code for this page

Was this helpful?