HRB1684301-12

Enabling/Disabling communication protocols and changing port numbers

Changing Ethernet communications using the display

See Setting up Ethernet communications using the display for instructions on how to enable/disable HTTP / HTTPS, DPWS, EtherNet/IP and DNP3 settings on your meter.

Changing basic Ethernet settings using the webpages

See Configuring basic Ethernet settings using the webpages for instructions on how to change the basic Ethernet settings of your meter.

Changing advanced Ethernet settings using the webpages

See Configuring advanced Ethernet parameters using the webpages for instructions on how to change the advanced Ethernet settings of your meter.

Changing BACnet/IP settings using the display

See Configuring BACnet/IP settings using the display for instructions on how to change the BACnet/IP settings on your meter.

Changing BACnet/IP settings using the webpages

See Configuring BACnet/IP settings using the webpages for instructions on how to change the BACnet/IP settings of your meter.

Enabling/Disabling DNP3 using the display

See Configuring DNP3 setting using the display for instructions on how to enable/disable DNP3 on your meter.

Enabling/Disabling DNP3 using the webpages

See Configuring DNP3 setting using the webpages for instructions on how to enable/disable DNP3 of your meter.

Enabling/Disabling Modbus TCP/IP filtering using the webpages

See Configuring Modbus TCP/IP filtering using the webpages for instructions on how to enable/disable Modbus TCP/IP filtering of your meter.

Changing SNMP settings using the webpages

See Configuring SNMP using the webpages for instructions on how to change the SNMP settings of your meter.

Enabling/Disabling FTP / FTPS using the display

See Enabling and disabling the FTP server using the display for instructions on how to enable/disable FTP / FTPS on your meter.

Enabling/Disabling FTP / FTPS using the webpages

See Enabling and disabling the FTP server using the webpages for instructions on how to enable/disable FTP / FTPS of your meter.

Enabling/Disabling the communication protocols and changing port numbers using the ION Setup

To enable/disable the HTTP / HTTPS, FTP / FTPS, DPWS, SNMP, DNP3, EtherNet/IP and BACnet/IP communication protocols using ION Setup, see the section for your meter in the ION Setup online help or in the ION Setup device configuration guide, available for download at www.se.com.

QR code for this page

Was this helpful?