HRB1684301-16

Instantaneous measurements

The meter provides highly accurate 1-second measurements.

These measurements include true RMS, per phase and total for:

  • 3-phase voltage (line-to-line, line-to-neutral)

  • 3-phase current, neutral and ground current

  • Active (kW), reactive (kVAR) and apparent (kVA) power

  • True PF (power factor)

  • Displacement PF

  • System frequency

  • Voltage (line-to-line, line-to-neutral) and current unbalance

The voltage and current inputs are continuously monitored at a sampling rate of 128 points per cycle. This amount of resolution helps enable the meter to provide reliable measurements and calculated electrical values for various commercial, buildings and industrial applications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?