HRB1684301-12

Logic alarm setup error prompts

Both the meter and ION Setup have error-checking provisions, and alert you with an error message if there is an error in the logic alarm setup.

You are alerted if the following actions are attempted:

  • The output of a logic alarm is used as an input to itself.

  • The same source is duplicated as another input on the same logic alarm.

  • The source register used is invalid or is a nonexistent parameter.

QR code for this page

Was this helpful?