HRB1684301-16

Monitoring waveform capture on meter’s webpages

NOTE: Refer to Restoration of temporarily disabled configuration settings in webpages to know availability of these features on your meter model.

Before you can view waveforms on the meter’s webpages, you need to perform some basic configuration using ION Setup to enable waveform capture and store the waveforms in COMTRADE format.

Manual trigger

1. Enable waveform capture on your meter

Set the status to Enable using ION Setup .

2. A waveform is captured when it is manually triggered using Modbus command or ION Setup

A COMTRADE record is generated and saved to your meter’s FTP / FTPS site.

3. View the waveform on the meter’s webpages

Login to the meter webpages.

Based on your meter firmware version, click Monitoring > General Monitoring > Waveforms to explore the waveform data.

Automatic trigger

1. Enable waveform capture on your meter

Set the meter’s nominal voltage and sag/swell parameters using ION Setup .

2. A waveform is captured when a power quality event occurs

A COMTRADE record is generated and saved to your meter’s FTP / FTPS site.

3. View the waveform on the meter’s webpages

Login to the meter webpages.

Based on your meter firmware version, click Monitoring > General Monitoring > Waveforms to explore the waveform data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?