HRB1684301-12

Notification icons

To alert you about meter state or events, notification icons appear at the top left or top right corner of the display screen.

Icon

Description

The wrench icon indicates that the power meter is in an over voltage condition or requires maintenance. It could also indicate that the energy LED is in an overrun state.

The alarm icon indicates an alarm condition has occurred.

The meter’s hardware and / or firmware lock is enabled.

(Displayed only in MID compliance meter models)

The icon indicates that a control power (auxiliary power) interruption event has occurred.

QR code for this page

Was this helpful?