HRB1684301-16

Reading device registers using the webpages

You can use the webpages to read a specified block of Modbus registers from the meter or from a slave device when the meter is acting as a gateway.
  1. Navigate to Diagnostics > Registers > Read Device Registers .
  2. Type the address of the device you want to read in the Device ID field.
  3. Enter values in the Starting Register and Number of Registers fields.
  4. Select data format of the registers you want to read from the Data Type field.
  5. Select the number format that you want to display the value of the registers in: Decimal, Hexadecimal, Binary, ASCII or Float.
  6. Click Read.

    Go to www.se.com and search for your meter’s Modbus register list to download a copy.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?