HRB1684301-16

Setting up logic alarms using ION Setup

Use ION Setup to configure logic alarms.
NOTE: You must first configure the alarms you want to use as inputs to a logic alarm. For example, if you use a standard (1-Sec) alarm as one of the inputs, you must set up its setpoint pickup, dropout and delay parameters.
  1. Select the logic alarm you want to set up, then click Edit.
  2. Select the alarms you want to use as inputs to the logic alarm.
  3. Click the double-arrow button to move the selected alarm(s) to the Selected  (max  4) box, then click OK.
  4. Configure the rest of the alarm setup parameters.
  5. Click OK then Send to save your changes to the meter.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?