HRB1684301-15

Digital input wiring considerations

The meter’s digital inputs require an external voltage source to detect the digital input’s on/off state.

The meter detects an on state, if the external voltage appearing at the digital input is within its operating range.

QR code for this page

Was this helpful?