DOCA0189EN–05

IP20 Optional Protection Cover

The IP20 protection cover is an optional protection cover which is used to cover the main power terminals between contactor and overload relay when mounted together.

The table below shows the compatibility of the protection cover with contactors and overload relays:

Contactor

Overload relay

IP20 cover reference

LC1G115-225

LR9G115–225

LA9G3704

LC1G265-500

LR9G500

LA9G3705

LC1G630-800

LR9G630

LA9G3706

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.