DOCA0189EN–05

Overload Protection of the Reverser

The thermal overload protection of the motor in a reverser can be provided by a TeSys Giga overload relay. The thermal overload relay rating is the same as the rating of the contactors.

The thermal overload relay can be mounted standalone and connected between the motor stator terminals and the contactors.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.