Map Arrow Element

A typical Layout includes a North Arrow, and Designer XI allows you to add one of your choosing. You need an image file of a North Arrow in a supported format to start, and the requirements are the same as for a standard Picture Element. The key difference between a regular Picture Element and a Map Arrow is that the Map Arrow Element rotates to match the angle of the map, while Pictures do not.

IMPORTANT: If there are multiple maps, the North Arrow respects the angle of the map that it is on top of. If the North Arrow is not on any map, it respects the angle of the largest map on the Layout page.

To create a Map Arrow Element, follow these steps:

  1. Ensure you have a canvas, as stated in Create Page Elements.

  2. Have your image ready in Windows Explorer. Later, you drag and drop it into the Create Element dialog.

  3. Click the Add Element tool.

  4. In the Add Element dialog, click Page Elements.

    IMPORTANT: It is required to click Page Elements first if you intend to create a new Element. If you are on Page Templates, then you would create a new Template.

  5. Click the Add tool.

  6. In the New Element Type dialog, click Map Arrow, then Next.

  7. In the Create Element dialog, type a concise and descriptive Name. This Name is seen by end users. This example uses “Standard North Arrow.”

  8. Notice the Category field. Categories organize your Elements. The first time you want a Category, you type its name into the field. For subsequent Elements, you can choose the Category name from the drop-down.

  9. Type a Category name. This example uses “North Arrows.”

  10. Type a Description. This is optional, but it allows you to provide a little more detail about the Element for your end users.

  11. Drag and drop your image file into position.

  12. Verify the image.

  13. Click Apply.

  14. Repeat with other Map Arrows, if necessary.

  15. When finished, click the Save icon.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.