HRB1684301-12

Setting up device log exports using the webpages

NOTE: Refer to Restoration of temporarily disabled configuration settings in webpages to know availability of these features on your meter model.

You can set up the meter to export its logs to a web server, either on a schedule or manually.

NOTE: Device log export times can vary, depending on the number of records to export. To avoid long log export times, consider reducing the logging frequency for the recorded items or selecting a more frequent log export schedule (e.g., weekly instead of monthly).
  1. Login to the meter webpages.
  2. Based on your meter firmware version, click Settings > Device Log Export OR click Settings > Communication > Device Log Export.
  3. Click Yes to Enable HTTP Device Log Export.
  4. Set the Frequency and configure the schedule as required.
    • Daily: select Daily to set the meter data log export to once a day. Use the Time of Day field to select what time the data log export occurs each day.
    • Weekly: select Weekly to set the meter data log export to once a week. Use the Time of Day and Day of the Week fields to select what time and day the data log export occurs each week.
    • Monthly: select Monthly to set the meter data log export to once a month. Use the Time of Day and Day of the Month fields to select what time and day the data log export occurs each month.
    NOTE: You can leave the default settings if you are exporting the data logs manually.
  5. Configure the HTTP parameters as appropriate.

    You can use the Test HTTP button to test the meter connection to the web server.

  6. Click Save changes or Apply Changes to send and save the new settings to the meter if you are configuring an export schedule, or click Manual Export to export the data logs immediately.

    Log export HTTP parameters available using the webpages

    Parameter Description

    Server IP Address *

    Enter the IP address of the server for the data log export.

    Server TCP Port *

    Enter the server port number for HTTP communications.

    Proxy Server IP Address *

    Enter the proxy server IP address, if required by your network.

    Proxy Server TCP Port *

    Enter the proxy server TCP port number, if required by your network.

    PATH

    Enter the network path of the folder where the data logs are to be exported.

    Field Name

    Enter the name of the exported data log.

    Host Name

    If using a virtual host name, enter the name here.

    Username

    Enter the username for accessing the server.

    Password

    Enter the password for accessing the server.

QR code for this page

Was this helpful?