Flexible Terminal Extensions
Flexible connecting bars can be used to connect TeSys Giga advanced or standard contactors with moulded case circuit breakers mounted in the same plane and orientation.
The table below provides the list of flexible terminal extensions used to connect advanced or standard contactors with moulded case circuit breakers:
Contactor |
Moulded case circuit breaker |
Number of poles |
Flexible terminal extensions |
---|---|---|---|
LC1G115-225 |
TeSys Power – Giga Motor Protection Frame 5 |
3P |
LA9G3111 |
ComPacT NSX100-250 |
|||
PowerPacT H- / J-Frame |
|||
ComPacT NSX100-250 |
4P |
LA9G4111 |
|
LC1G265-500 |
TeSys Power – Giga Motor Protection Frame 6 |
3P |
LA9G3112 |
ComPacT NSX400-630 |
|||
PowerPacT L-Frame |
|||
ComPacT NSX400-630 |
4P |
LA9G4112 |
|
LC1G630-800 |
ComPacT NS630b-1600 |
3P |
LA9G3113 |
PowerPacT P-Frame |
|||
ComPacT NS630b-1600 |
4P |
LA9G4113 |