Configuring SNMP using the webpages
You can configure your meter’s SNMP settings using the webpages.
- Login to the meter webpages.
- Based on your meter firmware version, click OR click .
- Modify the settings as required.
SNMP parameters available using the webpages
Parameter Values Description Enable SNMP
Yes / No
Enables or disables SNMP on your meter
System Contact
—
Enter the name of your SNMP administrator
System Name
—
Enter a descriptive name for your meter
System Location
—
Enter your meter’s location
Read-only Community Name / Write-only Community Name
—
Enter the community name used for SNMP requests
NOTE:It is highly recommended to set a community name that best meets your security guidelines. The community Name must contain between 8 and 16 characters with at least 1 uppercase, 1 lowercase and 1 special character.
*The special characters allowed are “@#$%&”.
Enable SNMP Traps
Yes / No
Enables SNMP trapping on your meter
Trap Receiver 1 IP Address / Trap Receiver 2 IP Address
—
Enter up to 2 trap receiver IP addresses where trap messages are sent
*Available only in latest firmware versions: -
PM5560 / PM5562 / PM5562MC / PM5563 / PM5580 meter models: 4.0.0 or later
-
PM5570 / PM5660 / PM5760 meter models: 6.0.0 or later
-
PM5650 meter model: 4.10.0 or later
-
PM5561 meter model: 12.0.0 or later
-
PM5661 / PM5761 meter models: 14.0.0 or later
-