HRB1684301-12

PM5500 / PM5600 / PM5700 meter models and accessories

The meter is available in several different models with optional accessories that provide various mounting options.

Meter models

Model Commercial reference Description
PM5560 METSEPM5560 Front panel mount, integrated display, 96 x 96 mm form factor, fits in a 1/4 DIN mounting hole.
PM5561 METSEPM5561 Same as PM5560, except the meter is calibrated to comply to strict MID standards.
PM5562

METSEPM5562

Same as PM5560 with the addition of a sealable hardware lock which prevents modification of revenue related settings and functions.
PM5562MC

METSEPM5562MC

Same as PM5562, except that it is sealed at the factory.
PM5563 METSEPM5563 Transducer (TRAN) model, no display, mounts on a standard TS35 top hat style DIN rail.
PM5563RD METSEPM5563RD Same as PM5563, except that it is package with a remote display (PM5RD).
PM5650 METSEPM5650 Same as PM5560 with the addition of sag/swell detection and waveform capture.
PM5580 METSEPM5580 Same as PM5560, except for 20 – 60 V DC control power (LVDC).
PM5570 METSEPM5570 Front panel mount, integrated display, 96 x 96 mm form factor, fits in a 1/4 DIN mounting hole with two digital inputs and two analog inputs.
PM5660 METSEPM5660 Front panel mount, integrated display, 96 x 96 mm form factor, fits in a 1/4 DIN mounting hole with two digital inputs and two RCM inputs.
PM5661 METSEPM5661 Same as PM5660, except the meter is calibrated to comply to strict MID standards.
PM5760 METSEPM5760 Same as PM5660 with the addition of sag/swell detection and waveform capture.
PM5761 METSEPM5761 Same as PM5760, except the meter is calibrated to comply to strict MID standards.

Meter accessories

Model Commercial reference Description
PM5RD METSEPM5RD

The remote meter display can be used with DIN meters. It has the same buttons, icons and LEDs as the display on an integrated meter, and is powered by the connection to the DIN meter.

NOTE: A remote display cannot be used with meters that have an integrated display.

See the PM5500 / PM5600 / PM5700 catalog pages, available from www.se.com, or consult your local Schneider Electric representative for information about mounting adapters available for your meter.

QR code for this page

Was this helpful?