MTN6215-0410S_SW_EN_EU_2024_06_05

Object Datatype of the Setpoint

Set the adjustment method of the setpoint temperature. You can choose whether to send 1-byte offset (Value in °C, DPT 5.010) or absolute temperature value (Float value in °C, DPT 9.001).

Function 1

Object datatype of setpoint

Setpoint temperature adjustment step

1 bit

2 bytes

1 °C

0,5 °C

1 °C

You should always set the minimum setpoint value below the maximum. Available range is 5°C to 37°C.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?