MTN6215-0410S_SW_EN_EU_2024_06_05

FCU Fan Function

Selecting FCU controller as the room temperature control function, you can also control a KNX fan coil actuator.

Function configuration

FCU controller

Fan

Fan level

1/2/3

Fan speed output setting

1-bit object function for fan speed

Enable/Disable

1-bit object for fan speed off

Enable/Disable

 

Fan speed auto. control function

Disable

Local controller

External controller

In addition to control, you set a fan speed during ongoing operation for manual mode and change between automatic and manual mode. In automatic mode, the fan coil actuator takes over control of the fan speed.

You define the thresholds for display of a fan step. In addition, you select the value for changing over between manual and automatic mode.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?