MTN6215-0410S_SW_EN_EU_2024_06_05

Air Quality Display

With Air quality display function, you can choose which air characteristic you want to display on the screen. The information comes from the sensor or KNX gateway or another KNX device that can send it to the KNX bus in a specified data point.

Express settings

Function

Air quality display

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication

Green/White

It can be temperature, humidity, or degree of pollution. You can also monitor the brightness (of the room or outside, depending on the type of your sensor).

Function 1

Type of air quality display

Int. temperature

Ext. temperature

Humidity

PM2,5

PM10

VOC

CO2

Brightness (lux)

Object datatype

Percentage (DPT 5.001)

Percentage (DPT 5.004)

 

Max. volume value

10 – 100 %

Each characteristic has its own unit. Either it is fixed (temperature – ° C, humidity – %). For other characteristics, you can name the unit yourself (PM2.5, PM10, VOC, CO2).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?