MTN6215-0410S_SW_EN_EU_2024_06_05

Floor Heating Controller

The settings for underfloor heating are the same as those for heating with the FCU controller. See FCU Controller.

The Interface display temperature parameter displays the actual indoor temperature by default. The Default set temperature parameter represents the initial temperature value you set.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?