MTN6215-0410S_SW_EN_EU_2024_06_05

Filter Time Counter

You can set the operating time in hours, after which the fan filter change alarm should trigger. Enable Filter time counter and choose the change time.

Function 1

Filter time counter

Enable

Evaluation time

100 – 1000 h

An audible alarm sounds when the filter change time has elapsed.

You can extend or reset the exchange time at any time in the ETS.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?