MTN6215-0410S_SW_EN_EU_2024_06_05

Pause for Change Slat Direction

To adjust the slats in the same direction incrementally, briefly press the button multiple times until you reach the desired position. The slats will continue to move in the same direction as long as you press the button within the adjustable pause time.

Once this pause time elapses, the slats will change their direction of rotation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?