Proximity Function
If you come within 12 cm of the device, the Proximity function triggers. The display switches on and switches off again after off delay elapses.
The Proximity function is activated by default. You can adjust the proximity triggering (default: built-in proximity sensor):
|
Proximity |
The Proximity function triggered via |
Never Proximity output object Proximity input object Proximity output or Proximity input object |
Value: Never
The function is deactivated.
The display is not affected.
Value: Proximity input object
The proximity function is triggered via the 1-bit Proximity input object.
The proximity object has the same function as the internal proximity sensor.
-
An On telegram activates the proximity state.
-
An Off telegram activates the no proximity state.
Value: Proximity output object
The proximity function is triggered via the internal proximity sensor. The internal sensor sends a 1-bit or 1-byte signal to the bus.
The proximity and no proximity states control the status indication.
Value: Proximity output or Proximity input object
The proximity function is triggered via the internal sensor or the external input object.
The sensor and the proximity object are linked to each other. The result of the link corresponds to an OR link.
If the proximity sensor detects no proximity, it sends a 0 telegram to the bus.