MTN6215-0410S_SW_EN_EU_2024_06_05

Operation Mode

Four operating modes (comfort, ECO, night and frost/heat protection), each with programmable setpoints, are available for differentiated control with different requirements.

During ongoing operation, you can temporarily move the setpoints within adjustable limits, or move them jointly for several operation modes.

Optionally, the basis for the setpoints can also be moved.

On the user interface, you can activate the comfort mode temporarily and set its duration.

Function 1

Operation mode

Enable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?