MTN6215-0410S_SW_EN_EU_2024_06_05

Venetian Blind Position and Slat

With the Venetian blind position and slat function, you can raise and lower a blind and adjust the slats.

Express settings

Function

Venetian blind position and slat

Function 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?