MTN6215-0410S_SW_EN_EU_2024_06_05

Scene Group Output Values

You can select the object type of the output value – 1 bit (switch), 1 byte (counter pulses) or 2 bytes (pulses), object value (0 is the default) and assign each output valve (1 – 6) a scene number to recall.

If you select 0, the valve remains inactive.

The Delay time for sending function allows you to set the required sending delay for each output valve so that you can set up specific scene recall sequences for each group output.

Scene group X

Gx: Output x function

   

Object type of output x

1 bit / 1byte / 2byte

 

1 – 6 → output x trigger scene NO. is

1 – 64 (0 = inactive)

   

Object value of output x

0 – 65535

   

Delay time for sending

0 – 63 * 0,1 s

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?