Express Settings
In Express settings, you can configure individual screens. You choose the number of function icons and functions of each screen. You can also name them. The name you choose will appear in the left sub-menu under Express settings.
Later, you simply connect group addresses to the functions.
|
Express settings |
Number of function icons |
1, 4, 6 |
|
|
Screen X |
Interface preview |
||
|
Icon X & X set as |
1 function / 2 functions |
||
|
Screen name |
≤20 English or 6 Chinese characters |
The function menu depends on the number of function icons selected and the button configuration for each screen. The following table provides an overview of possible combinations.
|
Icons |
Functions |
|---|---|
|
1 icon |
No function Brightness dimming RGB dimming RGBW dimming Colour temperature dimming Venetian blind position and slat Air conditioner Room temperature unit Ventilation system Audio control |
|
4 icons 2 icons = 1 function |
No function Switch Brightness dimming RGB dimming RGBW dimming Colour temperature dimming Curtain step/move Roller blind step/move Curtain position Roller blind position Venetian blind position and slat Scene Value output Loop operation Multiple operation Weather information Energy monitoring Air conditioner Room temperature unit Ventilation system Audio control |
|
4 icons 2 icons = 2 functions |
No function Switch Scene Value output Loop operation Multiple operation Weather information Energy monitoring Air quality display |
|
6 icons 2 icons = 1 function |
No function Switch Brightness dimming Curtain step/move Roller blind step/move Scene Value output Loop operation Multiple operation Weather information Energy monitoring |
|
6 icons 2 icons = 2 functions |
No function Switch Scene Value output Loop operation Multiple operation Weather information Energy monitoring Air quality display |