MTN6215-0410S_SW_EN_EU_2024_06_05

Energy Monitoring

The Energy monitoring function monitors electricity consumption in kWh. Data is retrieved from the bus and displayed on the screen (max. 999 999 KWh).

Express settings

Function

Energy monitoring

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication

Green/White

You can set the time interval for requesting the external sensor.

Express settings

Object datatype of energy display

Value in kWh (DPT 13.013)

 

Text for unit

5 bytes allowed

 

Time period for request external sensor

0 – 255 (min)

After the device restarts, a read request status is sent to the bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?