Group Objects
If you select Fahrenheit as the unit, there is no object for this option. The sensor always measures in degrees Celsius, but the temperature in degrees Fahrenheit is displayed.
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
1053 |
Screen |
Screen locking |
1bit |
C,W |
1.003 enable |
|
1054 |
Screen |
Screen on/off |
1bit |
C,W |
1.001 switch |
|
1055 |
Screen |
Screen brightness |
1byte |
C,W |
5.001 percentage (0..100%) |
|
1056 |
Night mode |
Night mode input |
1bit |
C,W,T,U |
1.024 day/night |
|
1057 |
Security |
Password trigger, 1bit value/ 1 byte value/ scene NO. |
1bit/1byte |
C,T |
1.001 switch 5.010 counter pulses 5.001 percentage 17.001 scene number |