MTN6215-0410S_SW_EN_EU_2024_06_05

Screen Lock

The screen lock protects the device against unauthorized use. The lock is set using the bus. An activated lock continues even after the device is restarted.

General screen lock

You activate or deactivate the screen lock for ongoing operation. When activated, you can lock the screen pages of the device. You lock with the value "1" and release with the value "0".

NOTE: Once the screen is locked via bus, you can NOT unlock it locally.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?