MTN6215-0410S_SW_EN_EU_2024_06_05

Cooling

In the cooling control mode, the current actual temperature is compared with the current setpoint temperature. If the actual temperature goes above the setpoint temperature, this control difference is counteracted by issuing a setpoint which does not equal “0”.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?