MTN6215-0410S_SW_EN_EU_2024_06_05

General Settings

General settings apply to all the buttons. You can set general properties such as:

  • Bus behavior after voltage recovery

  • Display user interface

  • Proximity function

  • Temperature measurement parameters

In addition, you can choose which advanced functions you want to enable.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?