MTN6215-0410S_SW_EN_EU_2024_06_05

General

You can set the delay time for sending telegrams to the bus after the device power up and reset. The device initialization time is not included. Bus messages received during the delay period are recorded.

The delay setting prevents the bus from being overwhelmed by telegrams when the power is on again. The function also informs you that the bus is ready for communication and the devices are powered at the same time.

You can set up cyclic sending of signals from individual devices. When there is no signal received, the device either does not work or is missing.

General settings: General

Send delay after voltage recovery

0 – 15 s

 

Cyclic sending live signal

1 – 240 s, 0 = inactive

 

Delay time for exiting setting status

s

   

Long operation for screen after

s

   

Day/Night mode switch over

Via object/Depend on certain time

   

Time for switch to night/day at

hh:mm

You can also set the time interval after the setting is completed: For example, between the temperature of the set values and the current measurement temperature.

Example:

You want to set the 3-second return time to the function page after you complete the advanced settings of the temperature controller.

Set the Delay time for exiting setting status parameter to 3 seconds.

When you finish with settings, the setting page automatically switches to the function page 3 seconds after the idle starts.


You can set the length of the short and the beginning of the long press of the button. By default, long operation starts after 0,5 s.

You can set the day and night mode switching either via the object or to the exact time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?