MTN6215-0410S_SW_EN_EU_2024_06_05

Restoring Defaults

You can set the factory-specified defaults using the Default parameters service button in the ETS.

You can use the Default and Default parameters service buttons to switch all parameters back to the settings on delivery (following consultation). The ETS will then permanently delete all manual settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?