MTN6215-0410S_SW_EN_EU_2024_06_05

Weather Information

You can set the weather information as either wind speed (in km/h or m/s) or 1-bit sunny/rainy information.

Express settings

Function

Weather information

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication

Green/White

You can also set the time interval for requesting the external sensor.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?