MTN6215-0410S_SW_EN_EU_2024_06_05

Value Output

Value output function allows you to send values for different data types, specific data types and values defined by parameters.

Express settings

Function

Value output

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication

Green/White

You can set a different output telegram for each operation. There are always five options for setting the value:

  • 1 bit – 1.001 switch

  • 2 bit – 2.001 switch control

  • 4 bit – 3.007 dimming control

  • 1 byte – 5.010 counter pulses (0..255)

  • 2 bytes – 7.001 pulses

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?