MTN6215-0410S_SW_EN_EU_2024_06_05

Multiple Operation

The Multiple operation function allows you to send up to 4 different objects at the same time with a single button operation.

You can set the following:

  • Distinction between short and long operation

  • Reaction on short/long and press/release operation

  • Number of objects (1 – 4)

Multiple operation supports these object functions:

  • Switch – on/off - sends telegram depending on settings (Toggle/On/Off).

  • Blind – up/down - sends telegram depending on the settings.

  • Recall/Store scene – sends call/save scene telegram (Nr. 1 – Nr. 64).

  • Percentage/Unsigned value – sends percentage/raw telegram.

Each function has the enable or disable sending option (No reaction/Send value).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?