MTN6215-0410S_SW_EN_EU_2024_06_05

Requirements for Safe Operation

Knowledge of the basic rules for operating programs using Windows® is a prerequisite for operation.

The ETS is the software for the KNX system, and is not manufacturer-specific.

Knowledge of ETS operation is required. This also includes selection of the correct sensor or actuator, transferring it to the line and commissioning it.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?