MTN6215-0410S_SW_EN_EU_2024_06_05

ETS Operation

Tables with describe parameter settings in ETS.

The main setting items are on the left. The specific parameters and their value settings are on the right.

Extended settings

Device safety

 
 

Device safety

At object value "1"

     

At object value "0"

     

Disabled

   

Cycle time surveillance for Safety object (0 ... 255, unit = 1 s, 0 = inactive)

0

In the ETS, the device parameters are opened using the Edit parameters service button.

The user interface is divided into 2 sections: The tabs are on the left and the parameters on the right, together with their values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?