MTN6215-0410S_SW_EN_EU_2024_06_05

Loop Operation

With the Loop operation, you can send values stepwise or step-less. There are two modes, fixed step adjustment and preset value.

Express settings

Function

Loop operation

Screen 1

Function name

1 – 8 characters (≤20 English or 6 Chinese characters)

Function 1

Icon preview

 
   

Function icon

 
   

Colour of function icon indication

Green/White

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?