MTN6215-0410S_SW_EN_EU_2024_06_05

Output Object Type

The proximity and no proximity states control the Proximity output object.

The proximity output can be set as:

  • 1 bit object - sends values "1" or "0".

  • 1 byte object - sends an adjustable value.

Example

Proximity function triggered via: Sensor

Object type of output value = 1 bit

Reaction for proximity approaching: Send a value

Output value: proximity

Delay time for sending = 0 s


Reaction for proximity leaving: Send a value

Output value: no proximity

Delay time for sending = 10 s


The sensor detects you and the device sends an “ON” telegram immediately. 10 seconds after you leave the room, the device sends an OFF telegram.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?