Screen Settings
In the Screen settings, you choose how many screens you want to use to control the device. You can access the room functions via up to 9 function pages and configure each of them in the Express settings menu.
Sort the screens by preference. If you enable Use main screen function, you can set one of the screens as the main screen.
The following setting is the no-action delay (Call main screen after). After it elapses, the device switches back to the main screen. You can adjust the delay time as needed (default = 5 s).
|
Screen settings |
How many screens do you use |
1 – 9 |
|
|
Screen position 1 – 9 |
Screen 1 – Screen 9 |
||
|
Use main screen |
Enable/Disable |
||
|
Select main screen |
Screen 1 – Screen 9 |
||
|
Call main screen after |
5 – 255 s |
In the Customized icon sub-menu, you can select the number of icons and describe their function.